Physical examination of the Refrigerated Air Dryer / Chiller that is compliant with the revised refrigerant law (Freon emissions limitations law)
Dr. Dryer is near you!
The once-a-year Physical Examination that the refrigerated air dryer requires.
In Japan, CKD has prepared and fully supports the physical examination by Dr. Dryer for the health of your refrigerated dryer / chiller. Now, you too can be compliant with the revised refrigerant law (Freon emissions limitations law) !
* The refrigerated dryers and chiller fall under the "Section 1 Provision of Information on Inspection and Other Maintenance of Specified Maintenance Products"
In Japan, CKD has prepared and fully supports the physical examination by Dr. Dryer for the health of your refrigerated dryer / chiller. Now, you too can be compliant with the revised refrigerant law (Freon emissions limitations law) !
* The refrigerated dryers and chiller fall under the "Section 1 Provision of Information on Inspection and Other Maintenance of Specified Maintenance Products"
Flow of inspection and support
Installation of the components in a suitable location, preserving the environment of the installation area / maintenance.
Simple inspection, periodic examination
[ Dr. Dryer ]
Leakage prevention measures, ban on replenishing the refrigerant without conducting repairs.
Inspections, etc., done on components must be kept on record.
Reporting and Publicizing the Calculated Amount of Leaked Fluorocarbons
[Main items of inspection maintenance]
- Is the dew point of the air normal?
- Is the pressure normal?
- Is the voltage normal?
- Has the refrigerant been leaking?
- Are there any foreign debris clogging the equipment?
Inspection required CKD products
Type of inspection | Applicable components and scope | Inspection frequency | Inspection details | ||
---|---|---|---|---|---|
Simple inspection | All components using Freon: Refrigerated Air Dryer, Chiller (water cooler) | Once or more every 3 months | Inspector: No limitations (Desirable to have the advice of a specialist) 1.External inspection: abnormal noise and/or vibration of visible piping, damage, corrosion, rust, oil covering, etc. |
||
Periodic examination | Rated output of the compressor's electric motor : 7.5 kW or more |
Refrigerated Air Dryer |
From GT9710WV to | Once or more every 12 months | Inspector: Qualified specialist (inspector or observer) 1.Direct method: Confirm using the bubbling fluid method, electronic gas detection method 2.ndirect method: Compare with the regular evaporation pressure value using a measuring device, etc. 3.1, 2 combination |
GT7960W (Production terminated) |
|||||
GT7960WD (Production terminated) |
|||||
RDW-900D/F (Production terminated) |
|||||
Chiller (Water cooler) |
HYW3027(W) (Production terminated) |
||||
HYW5027(W) (Production terminated) |
|||||
HYW5060C(W), HYW5069C(W) (Production terminated) |
|||||
HYW6048(W) (Production terminated) |
|||||
HYW7096, HYW7035U (Production terminated) |